cancel
Showing results for 
Search instead for 
Did you mean: 

Mono chrome display with STM32 Nucleo-144

mdalal
Associate III

Hi,

I am looking for monochorme display which can be interfaced with STM32 Nucleo-144 board. I looked into TouchGFX but it supports colored display board with this STM32 Nucleo-144 board. 

Can you suggest any monochomre display based board here?

https://www.st.com/en/evaluation-tools/nucleo-u575zi-q.html

Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @mdalal ,

Need to select first an LCD display on the market and find if it does have any available interface compatible with U5 product: FMC, SPI, I2C etc .. Some displays can be driven directly by GPIOs .. 

TouchGFX runs on any kind of display, and is not dependent on display technologies, interfaces, viewing angles, brightness etc but these are the display resolutions recommended for TouchGFX to achieve the intended performance: (according to this Link)

SofLit_0-1725966430873.png

 


@mdalal wrote:

Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?


There is no ready to use example STM32 Nucleo-144 board with a monochrome display.

See also these threads:

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-to-configure-touchgfx-with-a-monochrome-lcd-on-fmc/td-p/583195

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/basic-touchgfx-project-with-monochrome-spi-e-paper-display/td-p/641466

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello @mdalal ,

Need to select first an LCD display on the market and find if it does have any available interface compatible with U5 product: FMC, SPI, I2C etc .. Some displays can be driven directly by GPIOs .. 

TouchGFX runs on any kind of display, and is not dependent on display technologies, interfaces, viewing angles, brightness etc but these are the display resolutions recommended for TouchGFX to achieve the intended performance: (according to this Link)

SofLit_0-1725966430873.png

 


@mdalal wrote:

Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?


There is no ready to use example STM32 Nucleo-144 board with a monochrome display.

See also these threads:

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-to-configure-touchgfx-with-a-monochrome-lcd-on-fmc/td-p/583195

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/basic-touchgfx-project-with-monochrome-spi-e-paper-display/td-p/641466

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.