2024-09-10 01:42 AM
Hi,
I am looking for monochorme display which can be interfaced with STM32 Nucleo-144 board. I looked into TouchGFX but it supports colored display board with this STM32 Nucleo-144 board.
Can you suggest any monochomre display based board here?
https://www.st.com/en/evaluation-tools/nucleo-u575zi-q.html
Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?
Solved! Go to Solution.
2024-09-10 04:09 AM - edited 2024-09-10 04:09 AM
Hello @mdalal ,
Need to select first an LCD display on the market and find if it does have any available interface compatible with U5 product: FMC, SPI, I2C etc .. Some displays can be driven directly by GPIOs ..
TouchGFX runs on any kind of display, and is not dependent on display technologies, interfaces, viewing angles, brightness etc but these are the display resolutions recommended for TouchGFX to achieve the intended performance: (according to this Link)
@mdalal wrote:
Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?
There is no ready to use example STM32 Nucleo-144 board with a monochrome display.
See also these threads:
2024-09-10 04:09 AM - edited 2024-09-10 04:09 AM
Hello @mdalal ,
Need to select first an LCD display on the market and find if it does have any available interface compatible with U5 product: FMC, SPI, I2C etc .. Some displays can be driven directly by GPIOs ..
TouchGFX runs on any kind of display, and is not dependent on display technologies, interfaces, viewing angles, brightness etc but these are the display resolutions recommended for TouchGFX to achieve the intended performance: (according to this Link)
@mdalal wrote:
Also, whether TouchGFX provides any readymade example for the STM32 Nucleo-144 board with a monochorme display?
There is no ready to use example STM32 Nucleo-144 board with a monochrome display.
See also these threads: