2020-08-27 12:11 PM
The STM32G4xx Reference Manual (RM0440) Rev 4, Figure 2, "Memory Map" on Page 81 says Option Bytes 1 is from 0x1fff7800 to 0x1fff7810 (16 option bytes), Option Bytes 2 is from 0x1ffff800 to 0x1ffff810 (16 option bytes).
However:
Table 7 on page 94 says: Option Bytes 1 is from 0x1fff7800 to 0x1fff782f (48 option bytes) and Option Bytes 2 is from 0x1ffff800 to 0x1ffff82f (48 option bytes).
Is this discrepancy an error?
If not an error, please help me understand!!
Thanks kindly,
2020-08-28 2:31 AM
Hello @TwelveSquared ,
You are right. I raised your feedback internally to correct adresses in the Figure 2 "Memory Map" in RM0440:
So, 0x1FFF 7810 and 0x1FFF F810 will be updated to 0x1FFF 7830 and 0x1FFF F830.
Thank you for your contribution.
Best Regards,
Imen
2020-08-28 8:33 AM
Hello @Imen DAHMEN
Thank you for confirming and raising the issue internally. Looking forward to the corrected datasheet.
Thanks