2017-01-23 9:27 AM
Hello,
e.g. RM0377 lists the PWR_CR_LPDS bit unconditional for all L0X1 devices. * @version V1.7.1 headers define PWR_CR_LPDS only for L011 and L021. Is this right?
#stm32l02017-01-25 4:14 AM
Hi
Bonnes.Uwe
,In LPDS bit description in
, there is the following note: ' The LPDS bit is available on category 1 devices only'.Category 1 devices are STM32L011xx & STM32L021xx (see table 1 in the reference manual).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.