‎2021-11-17 06:46 AM
I would like to set up communication with a micro SD (or SD) card to save the data. I am planning to work with the NUCLEO card, I guess the communication is through the SPI interface. Do you know that libraries etc ...
Thanks for your helps
The nucleo card is NUCLEO-L433RC-P
Solved! Go to Solution.
‎2021-11-19 12:49 AM
Ok I'll do it :grinning_face:
‎2021-11-22 02:49 AM
Hi SofLit,
After unzip the folder 'en.stm32cubel4_v1-17-0_v1.17.0.zip' an when I open 'STM32CubeL4 under \Projects\STM32L476G-EVAL\Applications\FatFs\FatFs_uSD_Standalone' that you that you mentioned
I have several folder in this directory and which one I have to take to read with Notepad ++ ? Thank for your helps.
Regards
‎2021-11-22 02:56 AM
Hello,
Hope it's clear ..
‎2021-11-22 03:01 AM
I open the fles source and It's work ! Thank you