cancel
Showing results for 
Search instead for 
Did you mean: 

Merge the two half-duplex I2S in STM32F07X to 1 full duplex I2S

CWang.12
Associate II

I need to use the I2S of uC to communicate the Codec with the full duplex mode.Can I use the two half-duplex I2S in STM32F07X (e.g., STM32F071CBT7TR) to get that? I know that in the STM32F4 series, this function can be achieved with two half-duplex I2S.

4 REPLIES 4

Please don't put the entire post in the Title - see:

https://community.st.com/s/article/How-to-Post

Limit the title to ~ 70 characters.

You can edit it - use this button:

0693W00000QMNKRQA5.png 

#KeepTitleBrief

Yes. Use one as master, the other as slave, connect both clocks externally.

JW

Thanks,

But why modify the SPI/I2S resource for this functionality in the STM32F4x family?(The means of provision can be internal connect I2S_SCK, I2S_WS of 2 I2S together)

​In my opinion, Other than that ( connect both clocks externally), STM32F07x ( implements a full duplex I2S in the same way as STM32F4x. What else am I getting wrong?

Br​

Yes, it's a missed opportunity that woul make the 'F0​ family better, but it is what it is.

JW​