2022-07-28 3:37 AM
I need to use the I2S of uC to communicate the Codec with the full duplex mode.Can I use the two half-duplex I2S in STM32F07X (e.g., STM32F071CBT7TR) to get that? I know that in the STM32F4 series, this function can be achieved with two half-duplex I2S.
2022-07-28 4:10 AM
Please don't put the entire post in the Title - see:
https://community.st.com/s/article/How-to-Post
Limit the title to ~ 70 characters.
You can edit it - use this button:
#KeepTitleBrief
2022-07-28 4:13 AM
Yes. Use one as master, the other as slave, connect both clocks externally.
JW
2022-07-28 6:22 AM
Thanks,
But why modify the SPI/I2S resource for this functionality in the STM32F4x family?(The means of provision can be internal connect I2S_SCK, I2S_WS of 2 I2S together)
In my opinion, Other than that ( connect both clocks externally), STM32F07x ( implements a full duplex I2S in the same way as STM32F4x. What else am I getting wrong?
Br
2022-07-28 1:54 PM
Yes, it's a missed opportunity that woul make the 'F0 family better, but it is what it is.
JW