cancel
Showing results for 
Search instead for 
Did you mean: 

MCU temperature

Locnvselex_vn
Associate II

I'm working on a project with the STM32G4 MCU. I want to know the maximum temperature at which the MCU can operate at full power. What is the corresponding internal MCU temperature for that value?

Locnvselex_vn_0-1715518273613.png

What does the temperature information in the above image signify?

3 REPLIES 3
STOne-32
ST Employee

Dear @Locnvselex_vn ,

 

Maximum junction temperature TjMax for the part ending with 3 is 130Degree C and the ones by 6 will be 105 Degree for more details refer to this Application Note :https://www.st.com/resource/en/application_note/an5036-guidelines-for-thermal-management-on-stm32-applications-stmicroelectronics.pdf

you reach max Ambiant temperature up  XX degree but will depend on your package , Power ( I* V) and also PCB .

hope it helps you 

STOne-32

 

 

 

Locnvselex_vn
Associate II

so the maximum temperature at which the MCU can operate without performance being reduced ???

Andrew Neil
Evangelist III

Did you follow that link to Section 6.11: Thermal characteristics for further details?

AndrewNeil_0-1715693929091.png