User Activity

Hello everyone!During programming for the MCU STM32G431CbTx, I want to write a function to change the value of the "Break filter" bit for "Tim_BRK" as follows: static inline void mcu_protection_ov_enable_filter(){ uint32_t tmpbdtr = READ_REG(TIM1->...
I am using the Readout Protection Level 1 security method for the STM32G431 chip. However, after flashing the code, it doesn't work, and when I use the STM32Programmer software to check, I encounter an FF error like this. Can anyone help me with this...
I am using STM32G431cbtx and enabling RCC_MCO. Since the STM32G4 supports two pins, PA8 and PG10, PA8 is being used for another function, and I am using PG10 for RCC_MCO. However, when measuring the voltage on pin PG10, it is always high. Can anyone ...
I'm working on a project with the STM32G4 MCU. I want to know the maximum temperature at which the MCU can operate at full power. What is the corresponding internal MCU temperature for that value? What does the temperature information in the above i...
WRP cho phép cấu hình các vùng bộ nhớ Flash không thể ghi vào sau khi chúng đã bị khóa. Lõi xử lý chính (Cortex-M4) chỉ có quyền truy cập và thực thi mã nguồn trong các vùng bộ nhớ được bảo vệ bởi WRP??? Điều này đúng hay sai?
Kudos given to