Skip to main content
Associate
April 23, 2024
Question

MCU STM32G030K8T6 hangs

  • April 23, 2024
  • 14 replies
  • 5265 views

Hi all,

 

We have a product containing the STM32G030K8T6 MCU. The code is working like expected and the product is meeting all specifications. The product is battery powered and can be charged via USB. So far so good.

 

If the product is assembled it will go into a burn-in test where 70 plus products will be charged and de-charged between 3 to 10 times. During this test 1 to 3 products are failing, and with failing I mean the MCU just stops operation.

It stops at the following line of code:

Edit.png

 

We found a lot of high dV/dt on the powerline and think this is causing the MCU to hang although we cannot reproduce on a single piece.

If we test products randomly on bench or at our desk it doens't have any issues.

 

Currently we are at a dead end, does anybody has any suggestions?

 

This topic has been closed for replies.

14 replies

Tesla DeLorean
Guru
April 23, 2024

Make sure HardFault_Handler and Error_Handler output actionable data and assert a GPIO or LED rather than just while(1) silently. 

Make sure you're immediately ready to deal with interrupts coming from the TIM or other sources as you initialize pins and clocks.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
April 23, 2024

What development tools do you have?

It should be possible to connect to a running target without downloading & resetting:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/connecting-to-running-target/m-p/272666#M9437

 


@PLER wrote:

During this test 1 to 3 products are failing


Is consistently the same 1-3 which exhibit this "hang" ?

Is it consistent where in the test sequence the "hangs" start occurring?

 


@PLER wrote:

We found a lot of high dV/dt on the powerline and think this is causing the MCU to hang 


Have you tried addressing that?

ie, if you prevent the high dV/dt, do the failures stop?

 


@PLER wrote:

products will be charged and de-charged between 3 to 10 times.


So, apart from high dV/dt, you could also be having brown-outs? Have you looked into that?

 

EDIT:

What does it take to recover from a "hang" - just a reset? a full power-cycle? other?

 

Please use this button to properly post source code:

AndrewNeil_0-1713871411836.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PLERAuthor
Associate
April 23, 2024


@PLER wrote:

During this test 1 to 3 products are failing


Is consistently the same 1-3 which exhibit this "hang" ?

Is it consistent where in the test sequence the "hangs" start occurring?


It is random, there is no pattern.

 



@PLER wrote:

During this test 1 to 3 products are failing


Is consistently the same 1-3 which exhibit this "hang" ?

Is it consistent where in the test sequence the "hangs" start occurring?

 


@PLER wrote:

We found a lot of high dV/dt on the powerline and think this is causing the MCU to hang 


Have you tried addressing that?

ie, if you prevent the high dV/dt, do the failures stop?

 


@PLER wrote:

products will be charged and de-charged between 3 to 10 times.


So, apart from high dV/dt, you could also be having brown-outs? Have you looked into that?

 

EDIT:

What does it take to recover from a "hang" - just a reset? a full power-cycle? other?

 

Please use this button to properly post source code:

AndrewNeil_0-1713871411836.png

 

 


If I supply high dV/dt to a single product nothing happens to the product. The problem only arises at the burn in facility (which is not the same location), where they are connected in group to the same mains.

At our lab I made a test setup with the same simple USB charger. Interrupting the mains on an irregular base generates spikes which ripple further via the power path into the system. The ringing is visible on the Vdd of the MCU. Besides the ringing, the supply voltage is flat and stable.

In case the MCU comes into a hang state the only way to get out is by re-flashing the code. Resetting or power-cycling the MCU are not doing the job.

 

The occurrence of the error is very random, no pattern is visible. This makes it a very hard error to find.

 

The burn-in cannot be changed.


 
 
Andrew Neil
Super User
April 23, 2024

@PLER wrote:


In case the MCU comes into a hang state the only way to get out is by re-flashing the code. Resetting or power-cycling the MCU are not doing the job.

 

Can you read-back the flash content of a "hung" chip?

If so, does it verify against the original code image?

Does the code write to flash?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
April 23, 2024

In line 423, are you sure that pin named STATUS_LED_PIN should be in mode AF1_TIM3?

 

waclawek.jan
Super User
April 23, 2024

How are option bytes set? Namely, BOR_EN and BOR_LEV bits.

JW

PLERAuthor
Associate
April 24, 2024

It is confirmed to me that they are set.

Tesla DeLorean
Guru
April 23, 2024

BOOT0 pulled LOW or Floating?

Hung? Like a Latch-Up condition, or inexplicably dead in a while(1) loop, or in an infinite IRQ storm because the source hasn't been cleared? Ponder how you might determine this.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PLERAuthor
Associate
April 24, 2024

Boot0 is left floating, although it is connected to the TAG connector.

Andrew Neil
Super User
May 16, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.