2020-07-30 12:17 AM
In the general operating section, it is described as "Input voltage on RST and FT pins".
Do you consider the maximum rating of the RST pin to be the same as the FT pin?
2020-07-30 1:55 AM
Look in table 18 VIN:
Input voltage on RST and FT pins(8)
2 V < VDD < 3.6 V - 0.3 - 5.5
VDD < 2 V - 0.3 - 5.2