cancel
Showing results for 
Search instead for 
Did you mean: 

low lever driver backup sram example

Evan .1
Associate II

Is there an LL example to enable the backup ram.

This doesn't work:

   // Enable PWR clock

   LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);

   // Enable Backup ram clock

   LL_APB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_BKPSRAM);

   LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_RTCAPB);

   // Enable backup ram regulator

   LL_PWR_EnableBkUpAccess();

   LL_PWR_EnableBkUpRegulator();

   while (LL_PWR_IsActiveFlag_BRR() == 0);

   *(__IO uint32_t *) (BKPSRAM_BASE ) = 0x5A5A5A5A;

I can't find in the documentation what I forgot.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
26 REPLIES 26

I changed my code to this:

void CPU_config_backupram(void)

{

   volatile uint32_t test;

   RCC->APB1ENR |= 0x10000000;

   PWR->CR1 |= 0x00000100;

   RCC->AHB1ENR |= 0x00040000;

   test = PWR->CSR1;

   PWR->CSR1 |= 0x00000200;

   while( (PWR->CSR1 & 0x00000008) != 0x00000008) ;

   test = PWR->CSR1;

}

PWR->CSR1 is still 0x34000.

So are there any other requirements?

Reading variable: test gives me the following error message:

Multiple errors reported.

1) Failed to execute MI command:

-var-create - * test

Error message from debugger back end:

-var-create: unable to create variable object

2) Unable to create variable object

3) Failed to execute MI command:

-data-evaluate-expression test

Error message from debugger back end:

No symbol "test" in current context.

4) Failed to execute MI command:

-var-create - * test

Error message from debugger back end:

-var-create: unable to create variable object

To the only code other execute before CPU_config_backupram is STM32F767ZITX_FLASH.ld and this function is this:

void SystemClock_Config(void)

{

 /* Enable HSE clock */

 LL_RCC_HSE_EnableBypass();

 LL_RCC_HSE_Enable();

 while(LL_RCC_HSE_IsReady() != 1)

 {

 };

 /* Set FLASH latency */

 LL_FLASH_SetLatency(LL_FLASH_LATENCY_7);

 /* Enable PWR clock */

 LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);

 /* Activation OverDrive Mode */

 LL_PWR_EnableOverDriveMode();

 while(LL_PWR_IsActiveFlag_OD() != 1)

 {

 };

 /* Activation OverDrive Switching */

 LL_PWR_EnableOverDriveSwitching();

 while(LL_PWR_IsActiveFlag_ODSW() != 1)

 {

 };

 /* Main PLL configuration and activation */

 LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_HSE, LL_RCC_PLLM_DIV_8, 432, LL_RCC_PLLP_DIV_2);

 LL_RCC_PLL_Enable();

 while(LL_RCC_PLL_IsReady() != 1)

 {

 };

 /* Sysclk activation on the main PLL */

 LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);

 LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL);

 while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL)

 {

 };

 /* Set APB1 & APB2 prescaler */

 LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_4);

 LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_2);

 /* Update CMSIS variable (which can be updated also through SystemCoreClockUpdate function) */

 SystemCoreClock = 216000000;

}

Evan .1
Associate II

RCC->APB1ENR |= 0x10000000;

 PWR->CR1 |= 0x00000100;

 RCC->AHB1ENR |= 0x00040000;

  

 test = PWR->CSR1;

  

 PWR->CSR1 |= 0x00000200;

  

 while( (PWR->CSR1 & 0x00000008) != 0x00000008) ;

  

 test = PWR->CSR1;

This solved the problem. Somehow the debug environment uses an other image with the new source code?

All bus prescalers should be changed before increasing frequency. Why do you set APB1 and APB2 after the clock change?

Copied this from an UART example. So I assumed it worked correctly. So please tell me how it is done correctly.

Evan .1
Associate II

This seems the correct low level driver code for configure the backup ram:

void CPU_config_backupram(void)

{

// Enable PWR clock

   LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);

   // Enable Backup ram clock

   LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_BKPSRAM);

   // Enable backup ram regulator

   LL_PWR_EnableBkUpAccess();

   LL_PWR_EnableBkUpRegulator();

   while (LL_PWR_IsActiveFlag_BRR() == 0);

}

I literally told you it in my previous post!