cancel
Showing results for 
Search instead for 
Did you mean: 

LED pins STM32F415R

AMani.1
Associate

Hi there.

I am new to this, so do not judge me. Here is the question:

Which GPIO pins from STM32F415R (so the one with 64pins) I could use for lighting up a led?

Here is the documentation for it: https://www.st.com/resource/en/datasheet/stm32f415rg.pdf

Thank you!

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

Is this a custom board? Any GPIO pin can drive an LED at at least a few milliamps. Most pins can do 25mA, PHx and PC13-15 are less powerful.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

Is this a custom board? Any GPIO pin can drive an LED at at least a few milliamps. Most pins can do 25mA, PHx and PC13-15 are less powerful.

If you feel a post has answered your question, please click "Accept as Solution".
gregstm
Senior III

Yes. You can use most GPIO pins - and if you use high efficiency leds it is amazing how little power you need to drive them, so if your application requires long battery life you can get away with 1 milliamp or less. Red and yellow leds have a lower forward voltage drop (eg. 1.2V) and can allow the whole system to work at lower voltages (eg. 2.4V ).

I think it is sometimes helpful to work in reverse - think of all the other things you might want to use (eg. ADC, DAC, I2S, UART, wakeup pins,...) and choose GPIO pins that are not required by these peripherals. Nothing says "Hello World" better than a flashing Led - simple flashing leds has helped me debug many projects over the decades....