cancel
Showing results for 
Search instead for 
Did you mean: 

Laser sensor tw10sp not working correctly

Mbhir.1
Associate II

hello everyone, am working with the laser sensor tw10sp to mesure distance and interfacing it with UART. It require commands to work. i send the HEX command via UART and it response always with the same HEX number (clearly something wrong).

Any help please !!

0693W00000HqB96QAF.png

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

That's the same question you asked on the Arduino forum.

However, the laser module is not a product of STMicroelectronics, even if there is an STM32F030C8T6 on it. Maybe the description on Aliexpress will help you further?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

That's the same question you asked on the Arduino forum.

However, the laser module is not a product of STMicroelectronics, even if there is an STM32F030C8T6 on it. Maybe the description on Aliexpress will help you further?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Mbhir.1
Associate II

the sensor is communicating with the st board but the same HEX numbers are returning from it undependenly the command sent from the stm32. in the aliexpress description there is no explanation of such error..