2023-04-08 08:37 PM - edited 2023-11-20 08:40 AM
The MCU is NUCLEO-H7A3ZI-Q, and I used OSPI to drive w25q128. It is known that it can read and write normally. Then, I modified the sct file in Keil and completed the FLM file. Erase can proceed normally, but an error was reported when the Program reached 0x08000000. What should I do?
2023-04-09 09:32 AM
Address 08000000 is in the internal flash.
Ask the Keil support: https://community.arm.com/support-forums/f/keil-forum