2017-05-16 02:16 AM
Hello everyone:
i met a big problem, now i am using Nucleo L073RZ board and x-nucleo-ids01a5 expansion board to do the point to point communication. i want to use SPIRIT1 DK to receive and analyse the data. however, i can not open the com, it always shows the below figure, but my virtual ports have been installed correctly. could you please help me.
2017-05-16 03:19 AM
Hi
jay19930722
,Check if you follow all installation instructions and Firmwares upgrade as described in the
and QuickStartGuide with thehttp://www.emcu.it/Wireless/SubGHz/AN/SPIRIT1-SWandSDK_em.pdf
.Regards
Imen
2017-05-16 11:16 PM
Dear D:
so sorry to bother you again, i follow all installation instructions. however, the result is disappointed. i try to use another board to test whether i can use SPIRIT1 DK to open the com, but failed.it seems that virtual Com port of Nucleo-L073RZ is correctly connected to the PC, it may be the issues of spirit1 DK,the figure shows 'unable to detect GUI firmware', but i can not find GUI firmware in the SPIRIT1 DK installation package. then i tried to search GUI firmware on st.com but there are no discovery. the version of SPIRIT1 DK is 2.2.1, and my PC is win7 64 bits. whether i need to use old version or the latest SPIRIT1 DK could not be compatible with the Nucleo-Lo73RZ and X-Nucleo-IDS01A5.