cancel
Showing results for 
Search instead for 
Did you mean: 

issues of virtual communication of Nucleo board

jay zhang
Associate
Posted on May 16, 2017 at 11:16

Hello everyone:

i met a big problem, now i am using Nucleo L073RZ board and x-nucleo-ids01a5 expansion board to do the point to point communication. i want to use SPIRIT1 DK to receive and analyse the data. however, i can not open the com, it always shows the below figure, but my virtual ports have been installed correctly. could you please help me.0690X00000606xYQAQ.png0690X00000606z0QAA.png

2 REPLIES 2
Imen.D
ST Employee
Posted on May 16, 2017 at 12:19

Hi

jay19930722

,

Check if you follow all installation instructions and Firmwares upgrade as described in the

http://www.st.com/content/ccc/resource/technical/document/user_manual/cb/4c/21/61/a3/18/48/05/DM00092pdf/files/DM00092pdf/jcr:content/translations/en.DM00092pdf

and QuickStartGuide with the

http://www.emcu.it/Wireless/SubGHz/AN/SPIRIT1-SWandSDK_em.pdf

.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 17, 2017 at 06:16

Dear D:

so sorry to bother you again, i follow all installation instructions. however, the result is disappointed.  i try to use another board to test whether i can use SPIRIT1 DK to open the com, but failed.it seems that virtual Com port of Nucleo-L073RZ is correctly connected to the PC, it may be the issues of spirit1 DK,the figure shows 'unable to detect GUI firmware', but i can not find GUI firmware in the SPIRIT1 DK installation package. then i tried to search GUI firmware on st.com but there are no discovery. the version of SPIRIT1 DK is 2.2.1, and my PC is win7 64 bits. whether i need to use old version or the latest SPIRIT1 DK could not be compatible with the Nucleo-Lo73RZ and X-Nucleo-IDS01A5.