Hi, I'm developing audio recording system uinsg DFSDM of STM32L4. The microphone sound is converted to digital by external ADC and the converted data is sent via SPI to DFSDM. The problem is that the external ADC provides data but it has setup delay from rising edge of CKOUT and the data for DATIN isn't available at the time of riging edge of CKOUT. Is there any way to delay read timing of SPI so that it can wait setup delay? The setup delay of external ADC is about 58ns.