2024-08-27 6:44 AM
Hi Friends,
In STM32H7 MCU, both M7 and M4 can access shared memory, such as D3 SRAM4. I am going to use a D3 SRAM4 address as a place to share some status information between M7 and M4. If a 32bits word is defined shown as below, can the access from both sides(M7 and M4) be guaranteed atomic? Does it need HSEM?
-----
Code example:
volatile uint32_t *status_ptr = (status4_7 *)0x38000000;
In M4 side, *status_ptr = 0x1234abcd;
In M7 side, uint32_t status = *status4to7_ptr;
I know a 32bits word access is atomic in single core STM32 MCU.
Thank you in advance.
Solved! Go to Solution.
2024-08-27 9:08 AM - edited 2024-08-27 9:25 AM
It can't be safe if one core reads and the other writes as the operations are asynchronous. How could guarantee the consistency of the data between the cores? think about race conditions .. if the race condition doesn't matter in your application, you can do the operations without semaphore.
2024-08-27 6:57 AM
Yes, it's atomic. It won't read intermediate values.
2024-08-27 7:11 AM
It's dual-ported, writes are buffered and potentially cached. Assume RMW actions will NOT be atomic
>>I know a 32-bits word access is atomic in single core STM32 MCU.
That's a bit sweeping. An aligned write can be a single bus transaction. Peripherals should generally be treated as operating independently and concurrently.
2024-08-27 8:31 AM - edited 2024-08-27 8:47 AM
Hello,
If you mean by "atomic" to protect a variable from RW operations by the other core while performing a RW operation in the first core, I say yes, you need to use HSEM to lock/unlock RW operations. And you need also to define that memory region as Sharable region using MPU to prevent any data incoherency between CM7 and CM4 while using cache in CM7.
2024-08-27 8:51 AM
Thank you, SoftLit.
What if it is only written(W) in M4 side, and only read(R) in M7 side, can it be safe without using HSEM lock/unlock?
2024-08-27 9:08 AM - edited 2024-08-27 9:25 AM
It can't be safe if one core reads and the other writes as the operations are asynchronous. How could guarantee the consistency of the data between the cores? think about race conditions .. if the race condition doesn't matter in your application, you can do the operations without semaphore.
2024-08-29 8:18 AM
Hello @yhplx ,
Did your question has been answered? if yes please mark Accept as Solution the comment that answered your original question.
Thank you.
2024-08-29 8:28 AM
Carefully considered in can be relatively safe.
The hazards mostly being related to cache coherency and write buffering, operations would need to be fenced to ensure the content reached the memory cells before proceeding.
Just making something "volatile" is not sufficient.
I think one of the efficiencies would be to manage a larger buffer, or units of data, and then signal validity/availability via the HSEM/EXTI mechanics.
2024-08-29 8:47 AM
It gets to be more a completion issue. So think coherency, write buffering, fencing
There really isn't a clean atomic RMW at the MCU level, and if you do such things across multiple cores you tend to drag performance down to the lowest common denominator.
Make large buffers, using queuing methods.
Try to keep as much as possible on a single core, especially if you have data volume, and processing it would make it smaller, etc.
2024-08-30 1:42 AM
@Tesla DeLorean wrote:
Carefully considered in can be relatively safe.
The hazards mostly being related to cache coherency and write buffering, operations would need to be fenced to ensure the content reached the memory cells before proceeding.
Not obvious as you can imagine. Even with Strongly-Ordered you cannot grantee that as the access of the two cores is asynchronous and you can't guarantee at a given time which will operate on the memory.
Just making something "volatile" is not sufficient.
Indeed, there is no impact in there ..