2017-03-12 06:08 AM
The data sheet of the STM32F429 shows that its camera interface can take 14-bit parallel data and the maximum data rate is 54MB/s. Also it says the interface supports 8-bit progressive video monochrome or raw bayer format, without mentioning higher bitdepth. I wonder if it does imply that you can't capture 10-bit or 12-bit raw bayer image data with the DCMI.
2017-03-12 06:17 AM
I believe it is agnostic to the form of the data
2017-03-12 07:44 AM
The table 18 on the following document shows 14-bit raw bayer format is supported. But I'm not sure why the data sheet doesn't mention 10, 12, 14-bit.
Also it's strange that the ST wrote '8/10, 12, 14 bits progressive video (monochrome or raw bayer) '. What does '8/10' mean...? Why are there two same items in the 'supported data format' box?
2017-03-12 08:32 AM
8 or 10-bit modes