cancel
Showing results for 
Search instead for 
Did you mean: 

is tehre any simple way to create 5v tolerant ADC input on STM32H750?

BHell.1
Associate II

I have seen an example to create 5v tolerant input on STM32H750, a resistor divider controlled by GPIO. Now I can't find find it when I need it...anyone seen this example and maybe can point it out?

I suppose I need a buffer in front to avoind impedance matching problems?

thanks

1 REPLY 1
AScha.3
Chief II
  1. 2 resistors = a resistor divider
  2. buffer in front - only, if your divider cannot be driven by the source
If you feel a post has answered your question, please click "Accept as Solution".