2023-06-09 6:48 AM
I have a STM32H7 connected to a STM32L1 via RS485. I would like to use the H7 to reprogram the L1 using the system bootloader.
Has the USART to be full duplex?
Thank you, regards
Solved! Go to Solution.
2023-06-12 1:19 AM
I was a bit too quick with the previous answer: it may well be that the bootloader also communicates half-duplex via USART. The easiest way to check this is to test the various functions of the bootloader (connecting, flashing, reading, deleting, etc) with your setup, i.e. via USART, but with STM32CubeProgrammer.
Regards
/Peter
2023-06-09 12:31 PM
The system bootloader uses both lines, RX and TX for the USART, thus works full-duplex.
Details can be found in AN3155: USART protocol used in the STM32 bootloader.
Hope that helps?
Regards
/Peter
2023-06-12 12:15 AM
Hi Peter,
thank you for your quick reply!
We are using a MAX22025 (Half-Duplex RS-485/RS-422 Transceivers with AutoDirection Control), so we are able to use both USART pins, but we will not able to use them at the same time.
Is there any situation where there is the need of a simultaneously communication? Or where it is not know if the system bootloader is going to send something..?
Thank you,
regards
2023-06-12 1:19 AM
I was a bit too quick with the previous answer: it may well be that the bootloader also communicates half-duplex via USART. The easiest way to check this is to test the various functions of the bootloader (connecting, flashing, reading, deleting, etc) with your setup, i.e. via USART, but with STM32CubeProgrammer.
Regards
/Peter