cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use HW SS with multi-slave SPI mode?

HAlzo
Senior

Hello,

I am using DMA for one SPI slave with which requires SS Pulse mode.

Now I want to use two or more slaves

  • is it possible to use HW SS with multi slave "I think No"
  • is it possible to use HW SS for 1st slave and SW emulated SS using GPIO for the others?
  • Can the SW emulated SS can be controlled automatically from the DMA controller?

Best Regards

Hossam Alzomor

0 REPLIES 0