cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt Not Triggering for External Buttons on STM32H7S78-DK

Mehulrana511
Associate III

Hello,


I am currently working with the STM32H7S78-DK board using STM32CubeIDE for setup. I have connected four external buttons to the following pins: D2 (PF1), D4 (PF2), D7 (PF3), and D8 (PF4) on the board.

I have configured the buttons as external interrupts. However, while I am able to detect button presses in the main loop by polling the GPIO pins, the interrupt does not seem to trigger the HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) function.

Steps I have followed:

- Configured GPIO pins (PF1, PF2, PF3, PF4) as interrupt inputs in STM32CubeMX.
- Enabled the interrupts in the NVIC configuration.
- Implemented the HAL_GPIO_EXTI_Callback function in the code.
- Used GPIO_MODE_IT_RISING for interrupt triggering.
Despite the above configurations, the interrupt Callback is not being invoked when the buttons are pressed.

Here I attached some snapshot of configuration and code i have write.

Mehulrana511_0-1734093492542.png

Mehulrana511_1-1734093498365.png

 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stdio.h"
#include <string.h>

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart4;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
static void MX_GPIO_Init(void);
static void MX_FLASH_Init(void);
static void MX_UART4_Init(void);

#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)


GPIO_PinState buttonState[4] = {GPIO_PIN_RESET, GPIO_PIN_RESET, GPIO_PIN_RESET, GPIO_PIN_RESET}; // Variables to store button states

/* USER CODE BEGIN PV */

/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

void UART_Print(const char* message);
/* USER CODE END PFP */

/* USER CODE BEGIN 0 */
void UART_Print(const char* message)
{
   // Transmit the string data over UART
   HAL_UART_Transmit(&huart4, (uint8_t*)message, strlen(message), HAL_MAX_DELAY);
}

/* USER CODE BEGIN 0 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
    if (GPIO_Pin == BUTTON_1_Pin)
    {
    	UART_Print("BUTTON_1 pressed\r\n");
    }
    else if (GPIO_Pin == BUTTON_2_Pin)
    {
    	UART_Print("BUTTON_2 pressed\r\n");
    }
    else if (GPIO_Pin == BUTTON_3_Pin)
    {
    	UART_Print("BUTTON_3 pressed\r\n");
    }
    else if (GPIO_Pin == BUTTON_4_Pin)
    {
    	UART_Print("BUTTON_4 pressed\r\n");
    }

    HAL_GPIO_TogglePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin);
}

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Update SystemCoreClock variable according to RCC registers values. */
  SystemCoreClockUpdate();

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_FLASH_Init();
  MX_UART4_Init();
  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

	  	  buttonState[0] = HAL_GPIO_ReadPin(GPIOF, BUTTON_1_Pin);
	 	  buttonState[1] = HAL_GPIO_ReadPin(GPIOF, BUTTON_2_Pin);
	 	  buttonState[2] = HAL_GPIO_ReadPin(GPIOF, BUTTON_3_Pin);
	 	  buttonState[3] = HAL_GPIO_ReadPin(GPIOF, BUTTON_4_Pin);

//	 	  UART_Print("Hello from STM32!\n\r");
//	 	  printf("Hello_STM32!\n\r");
//	 	  HAL_Delay(1000);

	 	  for (int i = 0; i < 4; i++)
	 	  {
	 		if (buttonState[i] == GPIO_PIN_SET) // If the button is pressed
	 		{
	 			printf("Buttton %d is pressed\n\r",i);
	 			HAL_GPIO_TogglePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin);
	 		}
	 	  }

	 	  HAL_Delay(100);



  }
  /* USER CODE END 3 */
}

/**
  * @brief FLASH Initialization Function
  *  None
  * @retval None
  */
static void MX_FLASH_Init(void)
{

  /* USER CODE BEGIN FLASH_Init 0 */

  /* USER CODE END FLASH_Init 0 */

  /* USER CODE BEGIN FLASH_Init 1 */

  /* USER CODE END FLASH_Init 1 */
  /* USER CODE BEGIN FLASH_Init 2 */

  /* USER CODE END FLASH_Init 2 */

}

PUTCHAR_PROTOTYPE
{
  /* Place your implementation of fputc here */
  /* e.g. write a character to the LPUART1 and Loop until the end of transmission */
  HAL_UART_Transmit(&huart4, (uint8_t *)&ch, 1, 0xFFFF);

  return ch;
}

/**
  * @brief UART4 Initialization Function
  *  None
  * @retval None
  */
static void MX_UART4_Init(void)
{

  /* USER CODE BEGIN UART4_Init 0 */

  /* USER CODE END UART4_Init 0 */

  /* USER CODE BEGIN UART4_Init 1 */

  /* USER CODE END UART4_Init 1 */
  huart4.Instance = UART4;
  huart4.Init.BaudRate = 115200;
  huart4.Init.WordLength = UART_WORDLENGTH_8B;
  huart4.Init.StopBits = UART_STOPBITS_1;
  huart4.Init.Parity = UART_PARITY_NONE;
  huart4.Init.Mode = UART_MODE_TX_RX;
  huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart4.Init.OverSampling = UART_OVERSAMPLING_16;
  huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart4) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN UART4_Init 2 */

  /* USER CODE END UART4_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  *  None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOF_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOO_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pins : BUTTON_3_Pin BUTTON_2_Pin BUTTON_4_Pin BUTTON_1_Pin */
  GPIO_InitStruct.Pin = BUTTON_3_Pin|BUTTON_2_Pin|BUTTON_4_Pin|BUTTON_1_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_PULLDOWN;
  HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

  /*Configure GPIO pin : GREEN_LED_Pin */
  GPIO_InitStruct.Pin = GREEN_LED_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
  HAL_GPIO_Init(GREEN_LED_GPIO_Port, &GPIO_InitStruct);

  /* EXTI interrupt init*/
  HAL_NVIC_SetPriority(BUTTON_1_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_1_EXTI_IRQn);

  HAL_NVIC_SetPriority(BUTTON_2_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_2_EXTI_IRQn);

  HAL_NVIC_SetPriority(BUTTON_3_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_3_EXTI_IRQn);

  HAL_NVIC_SetPriority(BUTTON_4_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_4_EXTI_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  *   file: pointer to the source file name
  *   line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

Could you please help me resolve this issue or provide guidance on what might be missing from the configuration?

Thank you for your support.

Best regards,
Mehul

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

Getting back to you regarding this subject. It seems  the call of __HAL_RCC_SBS_CLK_ENABLE() was not generated by CubeMx.

Please add it manually in HAL_MspInit() in stm32h7rsxx_hal_msp.c file:

void HAL_MspInit(void)
{

  /* USER CODE BEGIN MspInit 0 */

  /* USER CODE END MspInit 0 */

  /* System interrupt init*/

  /* Enable the XSPIM_P1 interface */
  HAL_PWREx_EnableXSPIM1();

  /* USER CODE BEGIN MspInit 1 */
  __HAL_RCC_SBS_CLK_ENABLE();
  /* USER CODE END MspInit 1 */
}

 Hope that answers your question.

In meantime the team is working on it.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

10 REPLIES 10
SofLit
ST Employee

Hello,

Did you set break points in EXTI IRQ handlers? are they reached?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hi,

Thanks for answering.

No it is not reached to the  EXTI IRQ handlers.

/Mehul

I'm not seeing an issue with what you shared (except I'm missing something)!

Is that possible to zip your project and share it here?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Karl Yamashita
Principal

Show a schematic of how the buttons are connected to the STM32.

Also try testing the USER button on PC13.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Hi,
Please find attached link for my project.
UART_1.rar

/Mehul

Mehulrana511_0-1734323463284.png

After loading the program, an interrupt is generated without pressing the USER button (PC13) at starting. However, after pressing the button, no interrupt is generated. It is only detected by for loop "Button 4 is pressed".

here is my code,

 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stdio.h"
#include <string.h>

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart4;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
static void MX_GPIO_Init(void);
static void MX_FLASH_Init(void);
static void MX_UART4_Init(void);

#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)


GPIO_PinState buttonState[5] = {GPIO_PIN_RESET, GPIO_PIN_RESET, GPIO_PIN_RESET, GPIO_PIN_RESET, GPIO_PIN_RESET}; // Variables to store button states

/* USER CODE BEGIN PV */

/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

void UART_Print(const char* message);
/* USER CODE END PFP */

/* USER CODE BEGIN 0 */
void UART_Print(const char* message)
{
   // Transmit the string data over UART
   HAL_UART_Transmit(&huart4, (uint8_t*)message, strlen(message), HAL_MAX_DELAY);
}

/* USER CODE BEGIN 0 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
    if (GPIO_Pin == BUTTON_1_Pin)
    {
    	UART_Print("BUTTON_1 pressed\r\n");
    }
    else if (GPIO_Pin == BUTTON_2_Pin)
    {
    	UART_Print("BUTTON_2 pressed\r\n");
    }
    else if (GPIO_Pin == BUTTON_3_Pin)
    {
    	UART_Print("BUTTON_3 pressed\r\n");
    }
    else if (GPIO_Pin == BUTTON_4_Pin)
    {
    	UART_Print("BUTTON_4 pressed\r\n");
    }
    else if (GPIO_Pin == BUTTON_5_Pin)
	{
		UART_Print("BUTTON_5 pressed\r\n");
	}

    HAL_GPIO_TogglePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin);
}

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Update SystemCoreClock variable according to RCC registers values. */
  SystemCoreClockUpdate();

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_FLASH_Init();
  MX_UART4_Init();
  /* USER CODE BEGIN 2 */

  UART_Print("Hello from STM32 from UART4!\n\r");
  printf("Hello_STM32 from printf function!\n\r");

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */

	  buttonState[0] = HAL_GPIO_ReadPin(GPIOF, BUTTON_1_Pin);
	  buttonState[1] = HAL_GPIO_ReadPin(GPIOF, BUTTON_2_Pin);
	  buttonState[2] = HAL_GPIO_ReadPin(GPIOF, BUTTON_3_Pin);
	  buttonState[3] = HAL_GPIO_ReadPin(GPIOF, BUTTON_4_Pin);
	  buttonState[4] = HAL_GPIO_ReadPin(GPIOC, BUTTON_5_Pin);

//	  UART_Print("Hello from STM32!\n\r");
//	  printf("Hello_STM32!\n\r");
//	  HAL_Delay(5000);

	  for (int i = 0; i < 5; i++)
	  {
		if (buttonState[i] == GPIO_PIN_SET) // If the button is pressed
		{
			printf("Buttton %d is pressed\n\r",i);
			HAL_GPIO_TogglePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin);
		}
	  }

	  HAL_Delay(100);

  }
  /* USER CODE END 3 */
}

/**
  * @brief FLASH Initialization Function
  *  None
  * @retval None
  */
static void MX_FLASH_Init(void)
{

  /* USER CODE BEGIN FLASH_Init 0 */

  /* USER CODE END FLASH_Init 0 */

  /* USER CODE BEGIN FLASH_Init 1 */

  /* USER CODE END FLASH_Init 1 */
  /* USER CODE BEGIN FLASH_Init 2 */

  /* USER CODE END FLASH_Init 2 */

}

PUTCHAR_PROTOTYPE
{
  /* Place your implementation of fputc here */
  /* e.g. write a character to the LPUART1 and Loop until the end of transmission */
  HAL_UART_Transmit(&huart4, (uint8_t *)&ch, 1, 0xFFFF);

  return ch;
}

/**
  * @brief UART4 Initialization Function
  *  None
  * @retval None
  */
static void MX_UART4_Init(void)
{

  /* USER CODE BEGIN UART4_Init 0 */

  /* USER CODE END UART4_Init 0 */

  /* USER CODE BEGIN UART4_Init 1 */

  /* USER CODE END UART4_Init 1 */
  huart4.Instance = UART4;
  huart4.Init.BaudRate = 115200;
  huart4.Init.WordLength = UART_WORDLENGTH_8B;
  huart4.Init.StopBits = UART_STOPBITS_1;
  huart4.Init.Parity = UART_PARITY_NONE;
  huart4.Init.Mode = UART_MODE_TX_RX;
  huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart4.Init.OverSampling = UART_OVERSAMPLING_16;
  huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart4) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN UART4_Init 2 */

  /* USER CODE END UART4_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  *  None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOF_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOO_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pins : BUTTON_3_Pin BUTTON_2_Pin BUTTON_4_Pin BUTTON_1_Pin */
  GPIO_InitStruct.Pin = BUTTON_3_Pin|BUTTON_2_Pin|BUTTON_4_Pin|BUTTON_1_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_PULLDOWN;
  HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

  /*Configure GPIO pin : BUTTON_5_Pin */
  GPIO_InitStruct.Pin = BUTTON_5_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_PULLDOWN;
  HAL_GPIO_Init(BUTTON_5_GPIO_Port, &GPIO_InitStruct);

  /*Configure GPIO pin : GREEN_LED_Pin */
  GPIO_InitStruct.Pin = GREEN_LED_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
  HAL_GPIO_Init(GREEN_LED_GPIO_Port, &GPIO_InitStruct);

  /* EXTI interrupt init*/
  HAL_NVIC_SetPriority(BUTTON_1_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_1_EXTI_IRQn);

  HAL_NVIC_SetPriority(BUTTON_2_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_2_EXTI_IRQn);

  HAL_NVIC_SetPriority(BUTTON_3_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_3_EXTI_IRQn);

  HAL_NVIC_SetPriority(BUTTON_4_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_4_EXTI_IRQn);

  HAL_NVIC_SetPriority(BUTTON_5_EXTI_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(BUTTON_5_EXTI_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  *   file: pointer to the source file name
  *   line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

~Mehul

Hello @Mehulrana511 ,

Please avoid attaching files with other tools. The community supports files attachment up to 250M.

So please attach the project here using Drag and drop feature.

SofLit_0-1734512579819.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hi ,
Please find zip file of project I attached here,

Hello,

It's under internal investigation (internal ticket 199085).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.