cancel
Showing results for 
Search instead for 
Did you mean: 

Interfacing with I2C does not work in STM32F100xx Value line Discovery?Please help

Shri
Associate II

Hi all,I want to use the I2C of my STM32F100xx Low/Medium density value line Discovery board but without using STM32cube IDE because i want to learn the basic register initialization and each step necessary so that i can port it to any IDE but i am unable to get anything from my SCl and SDA pin.Here the code that i develop using IAR EWARM With the help of CD00246267.Point to note before this i interface GPIO as well as USART without any problem but in I2C didn't get any success.Here i am using PCF8574T as slave.Please help ..

#include <ST/iostm32f100xB.h>
void delay(void);
void i2c_init();
void I2c_sendata(char);
 
 
int main()
{
 i2c_init(); 
 while(1)
 {
 I2c_sendata('A');
 delay(); 
 }
 
void i2c_init()
{
  /**************************************************************************/
  //PB6(SCL) and PB7(SDA)
  I2C1_CR1_bit.PE=0;//disable pheripheral ,otherwise it is not allowed to make any changes in other register
  GPIOB_CRL_bit.MODE6=0x3;//Output mode, max speed 50 MHz
  GPIOB_CRL_bit.MODE7=0x3;//Output mode, max speed 50 MHz
  /*For bidirectional Alternate Functions, the port bit must be configured in Alternate Function Output mode (Push-Pull or Open-Drain). 
    In this case the input driver is configured in input floating mode*/
  GPIOB_CRL_bit.CNF6=0x3;//Alternate function output as open drain while input as floating
  GPIOB_CRL_bit.CNF7=0x3;//Alternate function output as open drain while input as floating
  RCC_APB1ENR_bit.I2C1EN=1;//Enable I2C1
  RCC_APB2ENR_bit.IOPBEN=1;//Enable clock of port b
  /**************************************************************************/
  
  I2C1_CR2=0x00000008;//APB set to 8MHZ  (other way 0b001000)
  I2C1_CR1_bit.ACK=1;//Enable Acknowledgement(Acknowledge returned after a byte is received (matched address or data)
  I2C1_CCR_bit.F_S=0;//Standard mode 0 /Fast mode 1
  /* In Sm mode, to generate a 100 kHz SCL frequency: If FREQR = 08, TPCLK1 = 125 ns so CCR must be programmed with 0x28(0x28 <=> 40d x 125 ns = 5000 ns.)*/
  I2C1_CCR_bit.CCR=0x28;
  /*In Sm mode, the maximum allowed SCL rise time is 1000 ns.If, in the I2C_CR2 register, the value of FREQ[5:0] bits is equal to 0x08 and
    TPCLK1= 125 ns therefore the TRISE[5:0] bits must be programmed with 09h */
  I2C1_TRISE=0x09;//TRISE[5:0] must be configured only when the I2C is disabled (PE = 0).Thaths why i write it before enabling PE of I2C1_CR1
  I2C1_CR2_bit.ITBUFEN=1;//this will enable flag for Tx buffer emepty,Rx buffer not empty
  I2C1_CR2_bit.ITEVTEN=1;//this will enable flag for SB(start bit sent when Master),stop bit received when slave(STOPF)
  // I2C1_CR1_bit.PE=1;//Peripheral Enable Register
  I2C1_CR1_bit.START=1;//Start/Repeated Start
  while(!I2C1_SR1_bit.SB);//wait for 
  //I2C1_DR=(0x20<<1)|(0x00000000);//send address and than write(Master Transmitter)
  I2C1_DR=0x40;  
  I2C1_CR1_bit.PE=1;
}
 
void delay(void)
{
int i = 1000000; /* About 1/4 second delay */
while (i-- > 0)
asm("nop");
}

 Note: I have checked the output with a logic analyzer its only displaying logic high.0693W000006G1f6QAC.png

5 REPLIES 5

Pretty sure the horse goes in front of the cart when it comes to synchronous logic and enabling the clocks.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Grant Bt
Senior

I'm not sure what's going on with your interrupt stuff (the "IT" parts), but you should PE enable the I2C before start or sending data.

i have enabled PE before start ,but still no change in output.i guess there is a problem in I2C1_CCR_bit.CCR=0x28; & I2C1_CR2=0x00000008;

but that i dont know how to calculate.any suggestion.thanks

can you please elaborate...thanks

The port is normally a GPIO, so to use any peripheral you need to enable the AFIOEN I think.