Interfacing with I2C does not work in STM32F100xx Value line Discovery?Please help
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-16 9:37 AM
Hi all,I want to use the I2C of my STM32F100xx Low/Medium density value line Discovery board but without using STM32cube IDE because i want to learn the basic register initialization and each step necessary so that i can port it to any IDE but i am unable to get anything from my SCl and SDA pin.Here the code that i develop using IAR EWARM With the help of CD00246267.Point to note before this i interface GPIO as well as USART without any problem but in I2C didn't get any success.Here i am using PCF8574T as slave.Please help ..
#include <ST/iostm32f100xB.h>
void delay(void);
void i2c_init();
void I2c_sendata(char);
int main()
{
i2c_init();
while(1)
{
I2c_sendata('A');
delay();
}
void i2c_init()
{
/**************************************************************************/
//PB6(SCL) and PB7(SDA)
I2C1_CR1_bit.PE=0;//disable pheripheral ,otherwise it is not allowed to make any changes in other register
GPIOB_CRL_bit.MODE6=0x3;//Output mode, max speed 50 MHz
GPIOB_CRL_bit.MODE7=0x3;//Output mode, max speed 50 MHz
/*For bidirectional Alternate Functions, the port bit must be configured in Alternate Function Output mode (Push-Pull or Open-Drain).
In this case the input driver is configured in input floating mode*/
GPIOB_CRL_bit.CNF6=0x3;//Alternate function output as open drain while input as floating
GPIOB_CRL_bit.CNF7=0x3;//Alternate function output as open drain while input as floating
RCC_APB1ENR_bit.I2C1EN=1;//Enable I2C1
RCC_APB2ENR_bit.IOPBEN=1;//Enable clock of port b
/**************************************************************************/
I2C1_CR2=0x00000008;//APB set to 8MHZ (other way 0b001000)
I2C1_CR1_bit.ACK=1;//Enable Acknowledgement(Acknowledge returned after a byte is received (matched address or data)
I2C1_CCR_bit.F_S=0;//Standard mode 0 /Fast mode 1
/* In Sm mode, to generate a 100 kHz SCL frequency: If FREQR = 08, TPCLK1 = 125 ns so CCR must be programmed with 0x28(0x28 <=> 40d x 125 ns = 5000 ns.)*/
I2C1_CCR_bit.CCR=0x28;
/*In Sm mode, the maximum allowed SCL rise time is 1000 ns.If, in the I2C_CR2 register, the value of FREQ[5:0] bits is equal to 0x08 and
TPCLK1= 125 ns therefore the TRISE[5:0] bits must be programmed with 09h */
I2C1_TRISE=0x09;//TRISE[5:0] must be configured only when the I2C is disabled (PE = 0).Thaths why i write it before enabling PE of I2C1_CR1
I2C1_CR2_bit.ITBUFEN=1;//this will enable flag for Tx buffer emepty,Rx buffer not empty
I2C1_CR2_bit.ITEVTEN=1;//this will enable flag for SB(start bit sent when Master),stop bit received when slave(STOPF)
// I2C1_CR1_bit.PE=1;//Peripheral Enable Register
I2C1_CR1_bit.START=1;//Start/Repeated Start
while(!I2C1_SR1_bit.SB);//wait for
//I2C1_DR=(0x20<<1)|(0x00000000);//send address and than write(Master Transmitter)
I2C1_DR=0x40;
I2C1_CR1_bit.PE=1;
}
void delay(void)
{
int i = 1000000; /* About 1/4 second delay */
while (i-- > 0)
asm("nop");
}
Note: I have checked the output with a logic analyzer its only displaying logic high.
- Labels:
-
I2C
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-16 1:09 PM
Pretty sure the horse goes in front of the cart when it comes to synchronous logic and enabling the clocks.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-17 9:48 AM
I'm not sure what's going on with your interrupt stuff (the "IT" parts), but you should PE enable the I2C before start or sending data.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-18 1:36 AM
i have enabled PE before start ,but still no change in output.i guess there is a problem in I2C1_CCR_bit.CCR=0x28; & I2C1_CR2=0x00000008;
but that i dont know how to calculate.any suggestion.thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-18 1:37 AM
can you please elaborate...thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-18 7:15 AM
The port is normally a GPIO, so to use any peripheral you need to enable the AFIOEN I think.