2024-07-07 10:15 PM - last edited on 2024-07-08 03:40 AM by mƎALLEm
i'm interfacing ADT7420 with STM32F411.
As per datasheet of ADT7420 the i2c specifications are as follows:
Table 2.
SCL Frequency 0 - 400 kHz
SCL High Pulse Width, tHIGH 0.6 μs
SCL Low Pulse Width, tLOW 1.3 μs
Therefore as per my understanding the i2c all operate in fast mode.
However, my doubt is related to duty cycle, the options available for i2c in stm32f411 are:
Tlow/Thigh=2
or
Tlow/Thigh=16/9
which option i have to use here
My code setting for i2c initilization are as follows
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 40000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
regards
2024-07-07 10:58 PM - edited 2024-07-07 11:01 PM
>which option i have to use here
Try with Tlow/Thigh=16/9 first .
And speed : Init.ClockSpeed = 40000; ? Try standard first, 100 k . 400k is next step...
And enable the noise filter(s) .
2024-07-08 10:28 AM
And enable the noise filter(s) .
plz tell me how to enable filters for i2c
2024-07-08 11:45 AM
here analog filter on, + dig.filter : if you wanna use, just set it: 0...15 possible.