cancel
Showing results for 
Search instead for 
Did you mean: 

Inspecting registers in IAR EWARM 8.22

Clonimus74
Senior II
Posted on June 24, 2018 at 11:17

Hi all,

I hope someone here can help.

When I debug my application (STM32L476QE) using IAR embedded workbench V8.22, I try to watch the NVIC registers

(View->Registers-> Rigisters 1, then right click and selecting 'View Group->Nested Vectored Interrupt Controller'), but all of their values are seen as 0x00000000 (even though that is not the actual value for sure).

What can be the problem?

The mapping of the resters within IAR are correct as seen in 'Project->SFR Setup'.

#iar-ewarm
2 REPLIES 2
Clonimus74
Senior II
Posted on June 26, 2018 at 11:08

No one encountered this?

Posted on June 26, 2018 at 14:58

>>No one encountered this? 

The lack of response suggest a lack of constituency, right?

Perhaps try working with IAR Support

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..