2019-04-11 05:10 AM
Hello everybody,
I want to measure the duty Cycle of a PWM Signal in Simulink. . I have managed it to generate a PWM signal with Simulink and STM32 MAT-Target. The problem is now when build a simple model to generate the code, the lines between the blocks will turn to red. and thus i am not able to measure the duty cycle with input capture direct mode. Can someone help with this?
BR
#Pwm-input-capture #Simulink #PWM #[STM32-Mat/Target] #Matlab #TIMER #