2021-04-07 2:30 AM
Hello!
A simple setup to run the ADC1 in continuous conversion mode runs as expected, but the measured values are incorrect as inspected via the debugger console. When connecting the ADC1 input pin to GND or 3.3V volts the measured value doesn't change as expected but always fluctuates around the decimal value of roughly ~14000.
The hardware I'm using is a custom discovery board from China according to the schematic:
https://github.com/mcauser/MCUDEV_DEVEBOX_H7XX_M/blob/master/docs/STM32H7XX_M_schematics.pdf
To discard issues with the hardware I verified the connectivity with a multimeter.
The problem persists when using other ADC channels/ input pins.
The code I used is:
int main(void)
{
#define ANALOG_IN 3
#define ADC_PA0_KANAL 16 // ADC1_INP16
RCC->AHB4ENR |= RCC_AHB4ENR_GPIOAEN; // PortA active
RCC->AHB1ENR |= RCC_AHB1ENR_ADC12EN; // dto. ADC_12
RCC->D3CCIPR |= RCC_D3CCIPR_ADCSEL_1; // per_clk ADC_12 enable
GPIOA->MODER |= ANALOG_IN; // PA0 analog IN
ADC12_COMMON->CCR = ADC_CCR_PRESC_3; // prescaler /32
ADC1->CR = ADC_CR_BOOST | ADC_CR_ADVREGEN ;
ADC1->SQR1 = ADC_PA0_KANAL << ADC_SQR1_SQ1_Pos; // input selection
ADC1->CFGR = (0b000<<ADC_CFGR_RES_Pos) | // 16 Bit
ADC_CFGR_JQDIS |
ADC_CFGR_OVRMOD |
ADC_CFGR_CONT; // continous conversion
ADC1->CR |= ADC_CR_ADEN |
ADC_CR_ADSTART;
uint32_t tmp;
while (1)
{
tmp = ADC1->DR;
}
}
What am I missing here? Is there a special setting to be considered because ADC1 and ADC2 are tightly couple?
2021-04-13 1:22 AM
So in the end I feel a little embarrassed about my question because in hindsight it seems rather clear. Anyways, in case someone got stuck at the same point and finds this post: the solution is to configure the ADCs channel preselection register PCSEL. For the example above one just has to add
LL_ADC_SetChannelPreSelection(ADC1, LL_ADC_CHANNEL_16);
or
ADC1->PCSEL |= (1UL << ADC_PA0_KANAL);
to the ADC configuration.
2022-07-01 4:02 AM
Hi
@CBrom.1
You got any solution for ADC issue.
I am facing same result conversion issue.
1) connecting 0V to channel 14 -> ADC result was half value of 16bit resolution (32767)
2) connecting 3.3v to channel 14 -> ADC result was full value of 16bit resolution (65535)
Setup:
CubeIDE : V1.10.0 Latest One
MCU : STM32H750VBT6
ADC : 2
Channel : 14
Method : Pulling Conversion
if you have any solution, could you please help to resolve it .
I am not to sure what to look for, i am struggling to solve it from past few days.
Thanks & Regards,
Ashvin Makwana