2023-07-24 05:10 AM
See Attached
Downloaded from web site as directed ;however download looks nothing like folder in the tutorial ;Placed comments in the comment section of the tutorial - so far no response - I asked for file structure as viewed in the tutorial . Download several times -same issue -Is this a corrupt folder or is there a way of activating the file - Cube MX ( located in the workspace )does not respond either
using F103,F446,F750 hardware however the issue is with the Interface of cube IDE and the folder ( file )
Solved! Go to Solution.
2023-07-25 04:10 AM
Issue Resolved the author did respond - Thank you
2023-07-24 06:05 AM
When you find something somewhere (github, various sites, blogs...) and it does not work - contact the author first. He/she may be glad to receive a feedback and maybe fix their stuff.
2023-07-25 04:10 AM
Issue Resolved the author did respond - Thank you