cancel
Showing results for 
Search instead for 
Did you mean: 

IMPORT PROJECT TO CUBE IDE -DEBUGGER HAMMER NOT RESPONSIVE GET "BUILD ACTIVE CONFIGUR.."

MROWL
Associate III

See Attached 

Downloaded  from  web site as directed ;however download  looks nothing like folder in the  tutorial ;Placed comments in the comment section of the tutorial - so far no response - I asked for file structure as viewed in the tutorial . Download several times -same issue -Is this a corrupt  folder or is there a way of activating the file - Cube MX ( located in the workspace )does not respond  either 

using F103,F446,F750   hardware however  the issue is with the  Interface of cube IDE and the folder ( file )

CanMultiTrouble2A.jpgCANMULTITROUBLE1A.jpg

1 ACCEPTED SOLUTION

Accepted Solutions

Issue Resolved  the author did respond - Thank you 

View solution in original post

2 REPLIES 2
Pavel A.
Super User

When you find something somewhere (github, various sites, blogs...) and it does not work - contact the author first. He/she may be glad to receive a feedback and maybe fix their stuff.

Issue Resolved  the author did respond - Thank you