Illogical EXTI code generation in CubeMX
Hi all,
I find the code generated by the CubeMX for EXTI line illogical.
Every EXTI ISR (e.g. EXTI0_IRQHandler, EXTI1_IRQHandler calls for the same function: HAL_GPIO_EXTI_IRQHandler, which in turn also calls for the same function: HAL_GPIO_EXTI_Callback.
That means that both must be re-entrant functions, which makes the implementation riskier.
With HAL_GPIO_EXTI_IRQHandler I understand, since it should not change and it relies on HAL_GPIO_EXTI_Callback.
The thing is that if I want to not rely on HAL_GPIO_EXTI_Callback and prevent using re-entrant code, I need to check the flag (__HAL_GPIO_EXTI_GET_IT) in the specific ISR (e.g. EXTI0_IRQHandler), the flag is checked in a not so logical place, in HAL_GPIO_EXTI_IRQHandler after some of my code was already executed in the specific ISR.
I would think a specific callback for each EXTI should have been generated to prevent the risk of re-entrancy.
Thoughts?