2017-10-31 3:25 PM
Hi group,
I have installed the AC6 Plugins in eclipse oxygen and try to create a test project for F3 Discovery.
I've choosen Standard Peripheral Library and pressed 'Download Firmware'.
There is something 32 MB downloaded and then installed but that seems to fail with
'Not able to establish connection to remote host !' but I think the message is wrong, something else fails.
I've tried another directory in the settings also, no luck.
Any ideas?
2017-10-31 4:26 PM
I now have installed the whole Ac6 IDE with the installer and has the same issue.
2017-11-02 4:37 AM
Hello
ingo.wolf
,Thank your for report this issue.This is reported internally to the appropriate team andunder investigation.
As recommended by
in the openstm32 Community, please use SW4STM32 V2.2 or use HAL libraries.Best Regards
Imen