cancel
Showing results for 
Search instead for 
Did you mean: 

Identifying Fake STM32

AScha.3
Chief III

Split from Black Pill: Debugging STM32F103RCT6 in Keil Fails to Enter main()


Hi @mÆŽALLEm  ,

 

just about your "not genuine" statement:

>- No "ARM " marking

Same here on a F103 by STM , should be genuine, because its st-link on a F3-discovery board !

>- There is a notch and a hole-like on one of the corners.

Exactly same "problem" for many users, using the chip in a rotated position, because they took the "big" point as pin 1 indication. Exactly this is on many H743ZI and H7A3Z chips , we have here.

Same on the F303 on the disco board, also " a notch and a hole-like on one " in the cornes.

So maybe all these are "fakes", also on the discovery board i have here, or

you take a little time and look at the products of the company you working at.

Then decide, what is fake or genuine...

If you feel a post has answered your question, please click "Accept as Solution".
3 REPLIES 3
mÆŽALLEm
ST Employee

@AScha.3 wrote:

Hi @mÆŽALLEm  ,

Same on the F303 on the disco board, also " a notch and a hole-like on one " in the cornes.


hole-like -> the circle looks like a hole and deeper than it should be. Nothing to do with STM32 packages:

mALLEm_0-1743602761058.png

No "ARM" but at least a QR code (already mentioned before)

In any case we don't support these Blue/Black pill boards as , by history & experience, don't feature a genuine STM32. 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@mÆŽALLEm  ,

so just a pic from one of the boards i just see around here in office:

has:

- no ARM logo (and for sure is big enough, LQFP144 )

- deep small hole , at pin 1; even 2 (!) others, a flat big and a flat, with extra plateau in center.

AScha3_0-1743603910937.png

+ made in TWN , obviously.

Now: fake or not ???

 

If you feel a post has answered your question, please click "Accept as Solution".

Here we are talking about STM32F1. You can open a new thread for this picture F4. <-- split to separate thread

Each product has its own marking and it's continuously changing.


@AScha.3 wrote:

- deep small hole


Not the same hole. The one he shared has a hole with a prominent cylinder from the bottom.

For the picture he shared I'm 99.99% it's fake.

Look at the the corners of the chip image he shared it has a notch in the bottom left of the corner. STM32 doesn't have a such particular "cut" in the corner.

mALLEm_1-1743609817662.png

And we know that STM32F1 was the most one targeted by the counterfeit.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.