2024-04-30 6:03 AM
Hello everyone,
I want to configurate the I2C channels as pull-up in STM32CubeIDE for STM32F103C8T6, but I couldn't set it.
It looks like in the attached image. It just shows n/a in configuration.
How I set it as pull-up?
Please inform me. Thanks.
2024-04-30 6:31 AM - edited 2024-04-30 9:10 AM
The internal pull-ups are not suitable for use as I2C bus pull-ups - you need to use external pullups.
EDIT:
See this post for the effect of too-high and too-low pullups:
https://electronics.stackexchange.com/a/473799
2024-04-30 9:05 AM
Hi @hdhdhd
Internal pull-ups are not recommended for I2C. Pull-ups must be adapted to the I2C bus speed and to the bus load.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-30 9:28 AM
Hi,
i just tried , yes, on F103 no pullups to set , only n/a .
But on F401 i tried also, here pullups possible :
So for pullups - take another cpu . :)
2024-04-30 9:30 AM - edited 2024-04-30 10:31 AM
@AScha.3 wrote:So for pullups - take another cpu . :)
Or just use the proper external pullups - the internal ones (when available) are likely to be too large.