cancel
Showing results for 
Search instead for 
Did you mean: 

I2C channels as pull-up in STM32F103C8T6

hdhdhd
Associate II

Hello everyone,

I want to configurate the I2C channels as pull-up in STM32CubeIDE for STM32F103C8T6, but I couldn't set it. 

It looks like in the attached image. It just shows n/a in configuration.

How I set it as pull-up? 

Please inform me. Thanks.

 

hdhdhd_0-1714481859079.png

 

4 REPLIES 4

The internal pull-ups are not suitable for use as I2C bus pull-ups - you need to use external pullups.

 

EDIT:

See this post for the effect of too-high and too-low pullups:

https://electronics.stackexchange.com/a/473799

 

FBL
ST Employee

Hi @hdhdhd 

Internal pull-ups are not recommended for I2C. Pull-ups must be adapted to the I2C bus speed and to the bus load.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!
AScha.3
Chief III

Hi,

i just tried , yes, on F103 no pullups to set , only n/a .

 

But on F401 i tried also, here pullups possible :

AScha3_0-1714494422254.png

So for pullups - take another cpu . :)

 

If you feel a post has answered your question, please click "Accept as Solution".

@AScha.3 wrote:

So for pullups - take another cpu . :)


Or just use the proper external pullups - the internal ones (when available) are likely to be too large.