cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to use the CAN interface of my nucleo board and found several examples about how to communicate over CAN between two STM32 boards. I would like to connect a Nucleo board over CAN to my PC. Like uart with Putty or REAlterm. I that possible?

MBooi.2
Associate
 
1 REPLY 1
SofLit
ST Employee

Dear @Community member​ ,

As I understood from your question, you need to let your Nucleo board a Bridge CAN/UART.

Yes it's possible and you need to add a CAN tranceiver for CAN communication. For PC communication you can use Virtual COM (UART through ST-Link).

SofLit

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.