cancel
Showing results for 
Search instead for 
Did you mean: 

I use the NUCLEO-L476RG board. ADC runs at 64 MHz and ADC has a 5.33 Msps maximum conversion rate with full resolution.

bahadirblt
Associate

I need to take 10 samples (10 Hz) per second. How can I set ADC configurations on CubeMX. I use the lowest sampling time (2.5 cycles), but the values I convert and use in ADC change very quickly.

Thanks for helps.

1 ACCEPTED SOLUTION

Accepted Solutions

You probably want to trigger ADC conversions ("External trigger conversion source") from a timer, suitably set so that it triggers 10 conversions per second.

JW

View solution in original post

1 REPLY 1

You probably want to trigger ADC conversions ("External trigger conversion source") from a timer, suitably set so that it triggers 10 conversions per second.

JW