2022-08-24 09:09 AM
2022-08-25 04:17 AM
Hi @tCHAP.1 ,
In the Knowledge base, we have the following 2 articles:
You can refer to them, and then please let me know if they were helpful for you or not.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-25 10:02 AM
Hello Amel
these are AWS and Azure examples but I want to try the default example that comes preloaded.
I am not able to open webpage..
my chrome version is latest 100.x
2022-09-05 09:03 AM
Hello @tCHAP.1 ,
I ran the example under this path:
STM32Cube_FW_U5_V1.1.1\Projects\B-U585I-IOT02A\Demonstrations\IOT_HTTP_WebServer\STM32CubeIDE
I did the following:
As a terminal I used Hercules
Mohamed Aymen
2022-09-06 05:40 AM
what web browser are you using to connect to the board's web server ?
2022-09-06 10:20 AM
I used chrome latest version on a windows laptop as well as on iPhone tried with chrome and safari
2022-09-06 10:21 AM
I tried this and after trying all available guidance on web I had no luck. I do get IP address from board but browser doesn’t open anything
2022-09-09 08:14 AM
Hello @tCHAP.1,
You need to be connected at the same wifi from where the IOT board is connected to, otherwise you can't open the web page with the provided IP address.
Mohamed Aymen
2022-09-09 08:59 AM
Thanks for your reply. For sure my other device is also connected to same AP. In fact I can ping to the module. It’s just that webpage not opening. I’m surprised that no one else has faced this issue.