cancel
Showing results for 
Search instead for 
Did you mean: 

I'm writing the following code: GPIOA-"MODER" 0x400; (set GPIO_MODER_MODE5_0). It's not working! In the debugging window, bit 11 doesn't change and the LD4 LED doesn't switch.

VTyut.1
Associate

I have Nucleo-G071RB. I want to flash the LED LD4 using CMSIS. Use IAR 8.40

I'm writing the following code: GPIOA->MODER |= 0x400; (set GPIO_MODER_MODE5_0). It's not working! In the debugging window, bit 11 doesn't change and the LD4 LED doesn't switch!

However, if I write a GPIOA->MODER = 0x400; then it works. (the debugger doesn't work because it's on GPIOA the same way, but it doesn't matter).

The same thing is happening at other ports B, C, ...

What's my mistake?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

The reset value of GPIOA->MODER is 0xEBFF FFFF; so both bits of MODE5 are already set, by ORing to them they can't change.

GPIOA->MODER = (GPIOA->MODER & ~GPIO_MODER_MODE5) | (1 * GPIO_MODER_MODE5_0);

JW

VTyut.1
Associate

My error was that I didn't look at the set default values in MODER registers (F0 series - ...00000000000, G0 series - ...11111111).

Thanks!

AA_EmbededLearner
Associate

Try this one:

1- First set the address of the GPIO->MODER Register

GPIO_MODER = (uint32_t*)0x48000000;

2- Set the MODER [9:8] = 0x1

*GPIO_MODER |= 0x400;