2022-12-28 3:18 AM
2022-12-28 7:02 AM
Read the messages displayed in the console pane - the problem should be described there.
2022-12-28 9:03 AM
CubeIDE ? Windows ? Did the install go properly? Does it work with any other boards?
Can you access the device via STM32 Cube Programmer ?
Consider Keil? The ST Cortex-M0(+) have a free license
2023-01-10 3:30 AM
the example codes are running fine and there is no problem in debug but when i write same code and debug the keil ide abruptly close. except examples from cubemx i am not able to run any other code on keil ide