cancel
Showing results for 
Search instead for 
Did you mean: 

B-WL5M-SUBG1 (MB1779B) and V3minie

dam74
Associate II

Hi,

i'm trying to work with Sigfox and MB1779B board.

I try to connect with cube programmer and V3miniE.

here is the log :

dam74_0-1739290535898.png

is there a procedure to connect to board ?

thank you

1 ACCEPTED SOLUTION

Accepted Solutions

Looks like you have removed JMP2!

If jumper removed, the VDD is disonnected from 3V3 so the STM32WL5MOCH6S has no power!

JMP2 can be used for current measurement.

 

aweber_schaller_0-1739352760597.pngaweber_schaller_1-1739352789242.png

 

View solution in original post

10 REPLIES 10
Andrew Neil
Super User

Please show your wiring between the V3miniE and the B-WL5M-SUBG1 (MB1779B).

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

dam74_0-1739302438228.png

 

Andrew Neil
Super User

are you sure you have that ribbon cable the correct way around?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

it's a foolproof device, isn't it ?

i'm working with a lsm100A, and it's ok.

thank you, I'm going to check wiring

Try using "Hardware reset" - the default setting is "Software reset"

aweber_schaller_0-1739349296438.png

dam74
Associate II

this is my conf :

dam74_0-1739351667054.png

 

dam74
Associate II

I've tried differents Modes....

Looks like you have removed JMP2!

If jumper removed, the VDD is disonnected from 3V3 so the STM32WL5MOCH6S has no power!

JMP2 can be used for current measurement.

 

aweber_schaller_0-1739352760597.pngaweber_schaller_1-1739352789242.png

 

dam74
Associate II

thank you very much for your help !