2017-03-30 12:18 PM
The board can't function properly, it can be downloaded using ST-LINK but the output doesn't match with the program I wrote. Is it because the oscillator? I watch the oscillator signal and it is different from the right board. The other DIY board has more problems besides the oscillator signal, the VCC pin voltage is 0 V and the reset pin voltage is 0 V. Can anyone help troubleshooting these problems? Thank you.
#stm32-stm32f4 #stm32f4-oscillator2017-03-30 12:40 PM
Start with a schematic of what you've actually created.
2017-03-31 2:37 AM
Hi
Az_Zahra.Itsna
,Have a look to the getting started hardware of your STM32 related product you find some Recommended PCB routing guidelines:
For more details on compatible crystals and hardware techniques on PCB, refer to
-Nesrine-