Skip to main content
Associate II
March 6, 2025
Solved

NUCLEO-H753ZI: Communication with PC

  • March 6, 2025
  • 3 replies
  • 2249 views

I'm trying to use my NUCLEO-H753ZI board to send some message to my PC using UART. I read from the data sheet that USART3 is connected to the ST-LINK for the Virtual COM Port (VCP), and USART3 can directly transmit messages to the PC. However, in the configuration window, USART3 is greyed out and cannot be configured. Is this normal? If so, how can I send messages to my PC using this board?

Screenshot 2025-03-06 at 21.54.57.png

This topic has been closed for replies.
Best answer by mƎALLEm

Hello @doronzzz and welcome to the community.

Because it is already configured in the Bsp and the code is already generated by CubeMx:

mALLEm_1-1741298737024.png

And you've selected to configure the VCP at the creation of the project based on the board:

mALLEm_0-1741298656269.png

Hope that answers your question

 

3 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
March 6, 2025

Hello @doronzzz and welcome to the community.

Because it is already configured in the Bsp and the code is already generated by CubeMx:

mALLEm_1-1741298737024.png

And you've selected to configure the VCP at the creation of the project based on the board:

mALLEm_0-1741298656269.png

Hope that answers your question

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
doronzzzAuthor
Associate II
March 6, 2025

The RX and TX pins of USART3 says they are under BSP control. Is this the reason why USART3 is unavailable?

mƎALLEm
ST Technical Moderator
March 6, 2025

Yes.

If you uncheck the "Virtual Com Port" check box option, USART3 will be available again.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.