cancel
Showing results for 
Search instead for 
Did you mean: 

MXCHIP EMW3080 on B-U585-IOT02A with Zephyr

stuart_rubin_ns
Associate II

Hello, I am using the B-U585-IOT02A board with Zephyr. I can't see how to use the MXCHIP EMW3080 Wi-Fi chip. Has anyone made this work? Thanks

4 REPLIES 4
Sarra.S
ST Employee

Hello @stuart_rubin_ns

for the WIFI module: you can get the firmware on this link and then follow the procedure describe in the UM to program the WIFI module.

Also, you can find more details in the datasheet provided by MXCHIP: EMW3080-DS0069EN.pdf

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Sarra, thank you for your reply. Unfortunately, my issue is specifically with using Zephyr. This board (B-U585-IOT02A) does have Zephyr support, but it's not obvious for how to use Wi-Fi with Zephyr. Do you have any information on that? Thank you.

Hi Stuart. Did you manage to get this working under Zephyr? I am using the STMH7S78-DK board and want to use WiFi with the MXCHIP EMW3080 but stubbed against the same wall as you. Thanks in advance.

Hi Sarra

reading the documentation from that link is not clear to me which fimrware to use when my board is not a Rev C could you please advise?