cancel
Showing results for 
Search instead for 
Did you mean: 

I dont success to get the 200uA consumption of stop mode for STM32F765

chrisPyres66
Associate III

Dear all,

I have a board with only the STM32F765VIT6 and I program through the stlink with a power supply of 3.3V (.

At start of program i tried

  • HAL_PWR_EnterSTANDBYMode() to get 3.5uA with success if before i disable overdrive with HAL_PWREx_DisableOverDrive()
  • HAL_PWR_EnterSTOPMode(POR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI) to get 200uA without success whatever i try to disable (Prefetch, overclocking mode with underdrive, voltage regulator)

Like i have any connected pin, i did not configure pin to analog input like adviced in AN4749.

I have got still 5mA, any default configuration help will be pleased.

Thanks,

1 ACCEPTED SOLUTION

Accepted Solutions
Uwe Bonnes
Principal III

I do not understand your remark "Like i have any connected pin, i did not configure pin to analog input like adviced in AN4749." You must configure every unused pin as analog! Otherwise floating inputs with draw substantial current.

View solution in original post

3 REPLIES 3
Uwe Bonnes
Principal III

I do not understand your remark "Like i have any connected pin, i did not configure pin to analog input like adviced in AN4749." You must configure every unused pin as analog! Otherwise floating inputs with draw substantial current.

chrisPyres66
Associate III

Thanks for your answer but i did it and it does not change the consumption

Here are my test code :

    SCB->VTOR = FLASH_BASE | 0x0;
 
    //HAL_DBGMCU_EnableDBGStandbyMode();
    HAL_PWR_EnableBkUpAccess();
 
    // ART Configuration
    __HAL_FLASH_PREFETCH_BUFFER_DISABLE();
 
    // Overclocking
    HAL_PWREx_DisableOverDrive();   // Disable the overdrive mode
    __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
 
    // Voltage Regulator
    HAL_PWR_DeInit();
    HAL_PWREx_EnableFlashPowerDown();
    HAL_PWREx_DisableBkUpReg();                     // Disable the backup regulator
    //__HAL_RCC_PWR_CLK_DISABLE();
    //__HAL_RCC_SYSCFG_CLK_DISABLE();               // APB2 Clock for EXT I
    //HAL_PWR_DisablePVD();                         // Disable the power voltage detector
    //HAL_PWREx_DisableMainRegulatorLowVoltage();
    //HAL_PWREx_DisableLowRegulatorLowVoltage();    // Disable the overdrive mode
 
    // GPIO Disable
    __HAL_RCC_GPIOA_CLK_DISABLE(); //__GPIOB_CLK_ENABLE();
    __HAL_RCC_GPIOB_CLK_DISABLE(); //__GPIOB_CLK_ENABLE();
    __HAL_RCC_GPIOC_CLK_DISABLE(); //__GPIOB_CLK_ENABLE();
    __HAL_RCC_GPIOD_CLK_DISABLE(); //__GPIOB_CLK_ENABLE();
    __HAL_RCC_GPIOE_CLK_DISABLE(); //__GPIOB_CLK_ENABLE();
 
    uint i;
    GPIO_InitTypeDef  GPIO_InitStructure;
    GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
    GPIO_InitStructure.Pull = GPIO_NOPULL;
    for (i=0;i<13;i++) {
        GPIO_InitStructure.Pin = i;
        HAL_GPIO_Init( GPIOA, &GPIO_InitStructure);
    }
    // PIN A13/A141 for pg
    GPIO_InitStructure.Pin = 15;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
    for (i=0;i<16;i++) {
        GPIO_InitStructure.Pin = i;
        HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
    }
    for (i=0;i<16;i++) {
        GPIO_InitStructure.Pin = i;
        HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
    }
    for (i=0;i<16;i++) {
        GPIO_InitStructure.Pin = i;
        HAL_GPIO_Init(GPIOD, &GPIO_InitStructure);
    }
    for (i=0;i<16;i++) {
        GPIO_InitStructure.Pin = i;
        HAL_GPIO_Init(GPIOE, &GPIO_InitStructure);
    }
 
    // clear global wake-up flag
    PWR->CSR2 &= ~(PWR_CSR2_EWUP6 | PWR_CSR2_EWUP5 | PWR_CSR2_EWUP4 | PWR_CSR2_EWUP3 | PWR_CSR2_EWUP2 | PWR_CSR2_EWUP1); // FREQUENCY CHRIS
    PWR->CR2 |= PWR_CR2_CWUPF6 | PWR_CR2_CWUPF5 | PWR_CR2_CWUPF4 | PWR_CR2_CWUPF3 | PWR_CR2_CWUPF2 | PWR_CR2_CWUPF1; // FREQUENCY CHRIS
 
    HAL_PWR_DisableBkUpAccess();
    HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
    //HAL_PWR_EnterSTOPMode((PWR_CR1_LPDS | PWR_CR1_LPUDS | PWR_CR1_FPDS | PWR_CR1_UDEN), PWR_STOPENTRY_WFI);
    //HAL_PWREx_EnterUnderDriveSTOPMode(PWR_LOWPOWERREGULATOR_UNDERDRIVE_ON, PWR_STOPENTRY_WFI);

chrisPyres66
Associate III

Dear all,

Effectively the secret for low power is to have all the unused pins in analog mode but without forgetting to enable the gpio port clock.

Here is the simple code finally :

 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOE_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
 
  /* GPIO ADC config*/
  GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4
                          |GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9 
                          |GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12|GPIO_PIN_15;
  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); // A13-A14 for PG
  GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4
                          |GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9 
                          |GPIO_PIN_10|GPIO_PIN_11|GPIO_PIN_12|GPIO_PIN_13 
                          |GPIO_PIN_14|GPIO_PIN_15;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
  HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
  /*Configure GPIO pins : PH0 PH1 */
  GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
  HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
 
  HAL_PWREx_EnterUnderDriveSTOPMode(PWR_LOWPOWERREGULATOR_UNDERDRIVE_ON, PWR_STOPENTRY_WFI); // 200uA
  //HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); // 0.450mA

Thanks