2022-08-24 12:41 AM
As you can see due to i can't receive the required ack from N2 node, N1 node It keeps sending the same message. Then HAL_ADDTX function returns HAL_CAN_ERROR_PARAM because the transmission is not happening and all mailboxes are full. Also i request TERR0 because of Transmission error of mailbox0.
Thank you in advance for your help.
2022-08-24 01:17 AM
Nobody has any idea what STM32 you're using or how anything is wired.
Guessing STM32F429-DISC board of some revision. Aren't the CAN pins conflicted?
Diagram the circuit, identify the pins, show the code.
2022-08-24 01:56 AM
I'm using STM32F429
Codes are in there:
2022-08-24 02:00 AM
And i'm reading this on logic analyzer CH1. Tx message cant transmitted so keep repeating.
2022-08-24 02:03 AM
I didn't use 120 ohms because my transciever module has it.