cancel
Showing results for 
Search instead for 
Did you mean: 

I can't receive the required ack bit from N2 node. So CAN message can't be transmit from N1 node.

SUrte.1
Associate II

0693W00000QONoQQAX.jpg0693W00000QONpYQAX.pngAs you can see due to i can't receive the required ack from N2 node, N1 node It keeps sending the same message. Then HAL_ADDTX function returns HAL_CAN_ERROR_PARAM because the transmission is not happening and all mailboxes are full. Also i request TERR0 because of Transmission error of mailbox0.

Thank you in advance for your help.

4 REPLIES 4

Nobody has any idea what STM32 you're using or how anything is wired.​

Guessing STM32F429-DISC board of some revision. Aren't the CAN pins conflicted?

Diagram the circuit, identify the pins, show the code.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
SUrte.1
Associate II
SUrte.1
Associate II

And i'm reading this on logic analyzer CH1. Tx message cant transmitted so keep repeating. 0693W00000QOOU2QAP.png

SUrte.1
Associate II

I didn't use 120 ohms because my transciever module has it.