2023-05-22 1:59 AM
2023-05-22 4:09 AM
Hello @Nsg1987,
Please check AN4776 paragraph 6.1
Also there is an example in STM32Cube package following this path : Examples\TIM\TIM_CascadeSynchro,\TIM_ExtTriggerSynchro\TIM_Synchronization
and \TIM_ParallelSynchro
I hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-22 4:09 AM
Hello @Nsg1987,
Please check AN4776 paragraph 6.1
Also there is an example in STM32Cube package following this path : Examples\TIM\TIM_CascadeSynchro,\TIM_ExtTriggerSynchro\TIM_Synchronization
and \TIM_ParallelSynchro
I hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-22 9:18 PM
Thanks Sarra.
The example gave idea about the same. But facing issue when Timer2 operates at 800 Hz and Timer 3 at 100 Hz. Output of Timer 3 remains high.
Is there any way to achive this?